Part Number: SN74HC4066 Other Parts Discussed in Thread: SN74AHC4066 , Tool/software: Hello,
we got PCNs from different sources, that stated SN74HC4066PWR to be obsolete from June '24. As this part is marked as active on TI website ( https://www.ti.com…
Part Number: SN74HC4066 Other Parts Discussed in Thread: TMUX1511 , TMUX1112 , CD74HCT4066 Hi team,
Could you please confirm the voltage compatibility of the part SN74HC4066 with 5V supply when we interface with 3.3V logic controller. The VOH & VOL of our…
Part Number: SN74HC4066 Other Parts Discussed in Thread: SN74LV4066A Dears,
Good day!
SN74HC4066DR is NRND. Would you please help to suggest a PTP recommendation? thanks.
Part Number: SN74HC4066 e2e,
May I know how to define the VIH/VIL/VMAX/VMIN when we use Vcc=3.3V ?
Could I use the proportion between 2V to 4.5V to calculate?
Thank you,
Adam
Part Number: SN74HC4066 Other Parts Discussed in Thread: CD74HC4066 , e2e,
My customer is looking for P2P drop in replacement for 74LVC4066PW and our cross reference device is SN74HC4066PW,
However , from the cross reference code it says these two device…
Part Number: SN74HC4066 Other Parts Discussed in Thread: TMUX6121 Hi Team
My customer is looking for analog switch (1:1 SPST) IC with below requirement.
Please advise recommended or close to the request devices.
1, Vdd > 6V
2, Output current > ± 5…
Part Number: SN74HC4066 Dear support,
About the characteristics of the currents mentioned page 5 of our datasheet, we have some difficulties to understand why the values at 25°C are above the ones over -40 to 85°C. Is it a mistake?
Could you…
Na Na,
I do not see an issue with the schematic you have above. If the SN74HC4066 device is the lowest cost solution for you it will isolate the I2C bus since the two EEPROMs can't be set different address.
Adam
Other Parts Discussed in Thread: SN74HC4066 Hi all. I would like to get the on-state resistance characteristic graph. (For example x:voltage, y:on-state resistance, temprature 0℃~40℃) If you have this data, please let me know it. My e-mail : ogane-s@clv.macnica…
Part Number: SN74CBT3125 Other Parts Discussed in Thread: TMUX1511 , SN74HC4066 As per its functionality, if NOE is low ,Aport = Bport.
But when simulation is done ,the waveform is not as accepted, meaning Aport = Bport.
Kindly help to resolve this issue…