Part Number: SN74HCS08-Q1 Tool/software: Hi team,
Our customer is looking for logic IC which can meet below requirements. Could you recommend logic IC at lowest cost for customer?
- Power supply: 5V
- Ch: 1ch, 2ch, 4ch
- Type: AND, NAND
- Input: 2 i…
Part Number: SN74HCS08 Tool/software: Hi team,
What does the VT range mean? Is it a range of chip by chip variation? If users operates without intermidiate state, user must send >3.15V as high and <0.9V as low?
Best regards,
Hayashi
Part Number: SN74HCS08-Q1 Tool/software: Hello experts,
As shown in datasets of hcs family, low power consumption, noise rejection, and supporters slow input are the characteristics of the family.
I can understood the latter two, but I am confused with…
Part Number: SN74HCS08 Other Parts Discussed in Thread: SN74LVC1G08 , SN74LVC1G97 Hi team,
My customer is using our SN74HCS08.
And they find in the datasheet the spec Δt/Δv is unlimited.
Could you please kindly help check why is it unlimited…
Part Number: SN74HCS08-Q1 There are two marking methods on the same edition, one is 9CAKGJK, the other is 9CAKG1K, what does the 1 and J mean respectively
Part Number: SN74HCS08 Hi,
We use 74hcs serie chips to solve the slow rise/fall time issue, because RC(R:30K C:0.22uf) is designed as the input of 74hcs08 to have a certain delay time.
We belive that the solw rise time is suitable for hcs chips as…
Part Number: SN74HCS08-Q1 Hi TI Expert,
May we know the VIH/VIL(xA/xB) & VOH/VOL(xY) parameter of SN74HCS08QPWRQ1 under 5V VCC?
It seems that the EC table does not cover this part.
Or how to judge those parameter if the datasheet doesn't mention.…
Part Number: SN74HCS08 Other Parts Discussed in Thread: SN74HCS09 Hi, i have project use IC M74HC09RM13TR TSSOP , i want know if Texas SN74HCS08DR can replace it.
My pcb boards are ready , because it must to be TSSOP version
Thank you!
Part Number: SN74HCS08-Q1 Hey Team,
My customer has a question, shown below. Can you help to break down the affect of slew rate on the operation of the gate?
"We have a question on the slew rates of the SN74HCS08-Q1 part. Does the slew rate of the inputs…