Other Parts Discussed in Thread: SN74HCS08 Hi Sir,
May I learn from you, do we have a simple solution which can keep output always low no matter input is high or low?
Thank you.
Edward Chen
Part Number: SN74HC08-Q1 Other Parts Discussed in Thread: SN74HCS08-Q1 , Hello team,
I am looking for SN74HC08QPWRQ1 pspice library model.
Can I get pspice.lib file for this?
I usually haven't seen model library for logic and wondering whether TI supports…
Hi Shreyas,
Thanks for your reply!
I will try to recommend SN74HCS08-Q1 to the customer, but I still don't know why the output pin will short to GND if unused input pin float and input transition rise time is larger. Could you please explain more detailed…
Hi Shu-Cheng,
We are actually coming out with a new family of logic devices that will have integrated schmitt-triggers on all inputs. Along with the SN74HCS74-Q1, we have the SN74HCS08-Q1 which is an AND gate with schmitt-trigger inputs.
Since the device…
Hi Tobias,
Yes, the recommended transition rates are there for a reason. TI can only guarantee performance of the device within the recommended operating conditions listed in the datasheet. If you drive the inputs slower than this, you could see unexpected…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…
FAQ: Logic and Voltage Translation > Input Parameters >> Current FAQ
This question comes up fairly often because the HCS logic family is specified only at 2V, 4.5V, and 6V.
The following min / max values are interpolated from the datasheet tables…