Part Number: SN74HCS125-Q1 Other Parts Discussed in Thread: SN74HCS125 , TINA-TI , SN74LVC1G17 Customer was asking for the PSpice model of SN74HCS125-Q1 for the simulation. Could you please help provide that? Thank you.
Part Number: SN74HCS125 Hi,
Good Day. Where can I find VIH and VIL values in datasheet of SN74HCS125? If not found on the datasheet, can you help us to provide the value of VIH and VIL? Please advise. Thank you very much.
Best Regards,
Ray Vinc…
Part Number: SN74HCS125-Q1 Hi, Team
Hope you are doing well!
From the datasheet of SN74HCS125-Q1, I can know the VT+max@2V/4.5V/6V.
But what if I want to know the VT+max corresponding to other Vcc values?
For example, when Vcc=3.3V(I think it…
Part Number: SN74HCS125-Q1 Other Parts Discussed in Thread: LMX2595 , SN74LVC125A-Q1 Outputs from the SN74HCS125-Q1 will be going off board through a 2m, 100-ohm cable. I cannot add anything on the receiving board which has a LMX2595 receiving the signals…
Part Number: SN74HCS125 Other Parts Discussed in Thread: SN74LVC125A , SN74AHCT1G125 , SN74LV125A , SN74AHC125 , SN74LV4T125 , TXU0304
Hi
I have 5V microcontroller and I am trying to run two 3.3V slave could you please let me know if this will work…
Part Number: SN74HCS125 Other Parts Discussed in Thread: SN74LV4T125 , SN74AHCT125 , SN74AHCT541 , SN74AHCT1G125 , TXU0104
We're looking for the 4ch buffer with VCC=5V, and the Input Voltage is from MCU 3.3V.
It looks SN74HCS125 is able to meet this…
Part Number: SN74AHC14 Other Parts Discussed in Thread: SN74HCS125
Tool/software:
Dear Technical Support Team,
The data sheets for the SN74AHC14 and SN74LV125APWR describe that "Latch-Up Performance Exceeds 250 mA Per JESD 17".
However, the SN74HCS125…
Part Number: SN74LVC125A-Q1 Other Parts Discussed in Thread: SN74LVC125A , SN74HCS125 Hi,
We are looking for a drop in repalcmeet of Nexperia item 74LVC125A.
It will be used as the I2S signal buffer of our tuner IC.
I2S BCLK = 3.107MHz
I2S WS…
Part Number: SN74HCS126 Other Parts Discussed in Thread: SN74HCS125 Tool/software: Hi expert,
Customer would like to use will be with the smallest package one, SN74HCS126DYYR.
However in the latest datasheet, SN74HCS126DYYR is not included in the…
Part Number: SN74LVC1G17 Other Parts Discussed in Thread: TLV1851 , SN74HCS125 Tool/software: I've used this logic buffer (schmitt trigger) to receive a discrete signal which voltage can go from +15V to 0V.
A 12Kohm resistor connected to +15V provides…