Part Number: ISOW1044 Other Parts Discussed in Thread: SN74HCS09 , SN74HCS157-Q1 , TMUX1112 , , ISO1044 Hello,
My customer wants to connect CAN communication using ISOW1014, SN74HCS157-Q1, and SN74HCS09 as shown below to implement a special function…
FAQ: Logic and Voltage Translation > Input Parameters >> Current FAQ
This question comes up fairly often because the HCS logic family is specified only at 2V, 4.5V, and 6V.
The following min / max values are interpolated from the datasheet tables…