Part Number: SN74HCS21 Tool/software: Hello.
This is Hyokun Kim.
I would like to know the High/Low level input voltage specifications of the SN74HCS21 product.
And please let me know the source and the data that contains that information.
…
Part Number: SN74HCS21 Hi all.
Is there Thermal derating curve of logic IC?
I would like to know Thermal derating of logic IC such as SN74HCS21.
Best Regard,
Ryusuke
Part Number: SN74HCS21 Tool/software: Hi,
We are using two channel AND gate in one of our circuits. Only one channel is used & the other one is completely not used. Is it okay to put all the inputs & output of the unused channel as no connection (NC…
Part Number: SN74HCS21-Q1 Other Parts Discussed in Thread: SN74LVC1G125-Q1 , SN74LVC1G126-Q1 , SN74LVC1G99-Q1 , SN74HCS21 Hi Expert,
I'm verifying the "AND" logic IC SN74HCS21-Q1 for our project. I found an abnormal phenomenon from this chipset. Showing…
Part Number: SN74HCS21-Q1 Other Parts Discussed in Thread: UCC21710 Hello experts,
I am using this 4 input AND logic for combining fault signal from my gate drives (UCC21710 - four numbers). The fault pin is open drain so we provided 4.7k pull up…
Part Number: SN74HCS21-Q1 Hello,
If Vcc = 5V, input pull up voltage is 5V, then how much series resistor value required at the input of SN74HCS21-Q1?
Regards,
Abhishek D.
Part Number: SN74HCS21-Q1 Hello TI Team,
The Part MPN SN74HCS21-Q1 has IBIS Model in Design and Development.
So, Can you provide me Pspice Model for the Same part number?
Thanks,
Gaurav Ingle.
Part Number: SN74HCS21 Hi Team,
My customer have a demand to monitor 6 negative input voltage, such as -8V,-7V,-6V... Each input may different, but it is negative.
If anyone of the negative larger than 0V, the system will receive an alarm. If all…