Part Number: SN74HCS244-Q1 Hi Expert,
May you kindly confirm what is the input high level threshold for OE_N pin? I cannot find in datasheet.
Thanks!
Ethan Wen
Part Number: SN74HCS244-Q1 Other Parts Discussed in Thread: SN65LVDT41 , SN65LVDT14 Hi team,
My customer wants to drive the SPI signal between two separate boards. There are four twisted pairs between these two boards and the length is 1m. The twisted…
Part Number: SN74HCS244-Q1 Hi team,
I want to choose a buffer which could provide delay time about tens of ns (<100ns) and this delay time could be configured. Do you have any recommendation? Thanks!
Robin
Part Number: SN74HCS244-Q1 In the d/s 6.5, there is a table saying Vt+ and Vt-. However, it doesn't say the 3.3Vcc and its switching threshold. Could you offer this value? or it's better to offer an chart as Vcc versus switching threshold.
It should…
Part Number: SN74HCS244-Q1 Other Parts Discussed in Thread: SN7404 , SN74LVC8T245 , SN74AHCT541 , SN74AHCT244 Hi,
In a board that I'm designing, I need to "convert" a 3.3V digital signal into a 5V digital signal. So, I think what I need is a non-buffer…
Part Number: SN74HCS244-Q1 Dear team,
I am looking for 74CBTLV3245-Q100 replacement, but I can't find same function device. Our SN74HCS244-Q1 has very similar function. Our device has two OE pins while 74CBTLV3245-Q100 only have one OE pin. Do we have…
Part Number: SN74HCS244-Q1 Hi,
I would like to use non-inverting open drain buffer for my digital I/O application. If possible, please suggest me some part numbers with integrated pull-down resistor. I/O is 3.3V.
Thanks!
Part Number: SN74HCS244-Q1 Other Parts Discussed in Thread: TMUX1308 , , SN74LVC125A , SN74LVC3G17 , SN74ABT541B-Q1 Hi:
I'd like to design 8 channels demultiplexer for JTAG (Jtag repeater).
Front-end use 4*TMUX1308 as demultiplexer.
(TDI, TDO, TCK…
Part Number: SN74LV14A Other Parts Discussed in Thread: SN74LV86A , SN74HCS244 Tool/software:
Are both of the two combinations shown in the diagram above OK?
Part Number: SN74LVC244A Other Parts Discussed in Thread: SN74HCS244 , SN74HCS541 , , SN74LV244A
Tool/software:
Hello TI Team,
We are using the SN74LV244, and observed that when a 3.3V PWM signal is applied to the input, both the input and output…