Other Parts Discussed in Thread: SN74HCT541 , SN74HCS244-Q1 Hi team.
I found 2 TI solutions SN74HCT541 and SN74HCS244-Q1. but has some question as below,
1. SN74HCT541 is P2P but the function block inside not the same.
2. SN74HCS244-Q1 seems same function…
There is no pin-to-pin replacement.
The only 8-bit buffer with Schmitt-trigger inputs is the SN74HCS244-Q1. If you want inputs and outputs on opposite sides of the package, use the SN74LV8151.
Other Parts Discussed in Thread: SN74HCS244-Q1 Hi,
We required Buffer which supports SPI lines. We want to connect the spi lines from controller to buffer and from buffer to cell monitoring IC. Its logic level is 5V. Please suggest us the buffer part …
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…
FAQ: Logic and Voltage Translation > Input Parameters >> Current FAQ
This question comes up fairly often because the HCS logic family is specified only at 2V, 4.5V, and 6V.
The following min / max values are interpolated from the datasheet tables…