Part Number: SN74LS14 Dear experts,
Our customer has a question, they wanna to know the range of It+. From the datasheet, the typ value is –0.14 mA, but not give the min and max value.
so it would be great if you could help us to give the range…
Part Number: SN74LS14 In one of our design, we are using SN74LS14 to read the status from the limit switch (3 pin devices - 1 Normally closed, 2-Normally open, 3-Common) in this common is always connected to logic 0 and Normally closed pin is connected…
Part Number: SN74LS04 Hello,
My customer is designing their board using SN74LS04NS.
They observed some undershoot at the output as follows.
They replaced SN74LS04NS by SN74LS14NS, then the undershoot at the output was reduced as follows.
…
Part Number: SN74LS14 Hi Team,
Please let us double confirm if land pattern for SN74LS14NSR recommended by TI is below, just in case ?
There is no land pattern drawing for NS package in datasheet of SN74LS14NSR, but found CAD data in http…
Part Number: SN74LS14 Other Parts Discussed in Thread: SN74LVC14A Hi,
I encountered a problem when I was trying to make an square wave oscillator using SN74LS14N.
From the technical document, it shows that the output voltage (VOH) is 3.4V.
However…
Part Number: SN74LS14 Other Parts Discussed in Thread: SN74HC14 I implemented the following circuit with a SN74LS14 chip but I got unexpected voltages across C10.
Suppose TIMER_START is initially at 0V, which means the voltage across C10 is approximately…
Other Parts Discussed in Thread: SN7414 , SN74LS14 , SN74AHC14 Hello,
I am a hobbyist interested in a Schmitt-trigger / comparator IC to trigger a N-type power Mosfet to light some LEDs.
I came across the SN7414 Hex Schmitt-trigger inverter and I…
Part Number: TMS320F28379D Other Parts Discussed in Thread: LAUNCHXL-F28379D , SN74LS14 , AMC1200 Hello to everyone,
I'm looking to measure grid frequency using cmpss and ecap module of TMS320F28379D but I've some problem with the accuracy.
First…