Part Number: SN74LV1T08 Hi
We find there are the error in the SN74LV1T08 datasheet, that the function Table is belong to Positive-OR Gate but not Positive-AND Gate, please kindly double check, thanks,
Part Number: SN74LV1T08 Hi, I’m looking at SN74LV1T08DBVRG4. The description and data sheet state this is a 2 input AND gate. However the functional diagram and logic table show OR gate behavior. Is the diagram and logic table in the data sheet incorrect…
Part Number: SN74LV1T08 Hi there,
After importing the SN74LV1T08, I added the symbol, but it doesn't seem to be functioning.
However, when I put the symbol for Logic_function and it works.
May I know why there are so many types in the modle and…
Part Number: SN74LV1T08 Other Parts Discussed in Thread: SN74LVC3G07-Q1
Hi team,
I am looking for an AND Gate with level translator from 3.3V to 5V for one of input signal. VCC will be 5V but input signal level will be +5V and +3.3V.
The SN74LV1T08…
Part Number: SN74LV1T08 Hi, Good day. Our customer is using the SN74LV1T08 and they want to know if the below setup will work. in my case, i am giving vcc as 1.8V and for AND gate inputs "one input is 1.8v another is 3.3v" so will it work as expected…
While Clemens is correct we do also have LV1T Gates such as the SN74LV1T08 That can accomplish one of the functionalities of SN74LVC1G57. Those gates can be found Here
Regards,
Owen
Part Number: SN74LV1T08SN74LV1T08 is an AND gate that is marketed as an excellent level shifter for high frequency and wide voltage range。 I am wondering what is the propagation delay between the input gates? how could we mitigate the delay between input…
Part Number: SN74LV1T08 Hi all,
For SN74LV1T08, we couldn't find in ti.com. (1-ch, 2-input).
Due to its unique VIH spec, SN74LV1T08 is competitive. Please help tell the ti.com this problem.
Roy
Part Number: SN74LV1T08 Other Parts Discussed in Thread: SN74LVC1G08-Q1 HI BU team
Would you help suggest the part # with Q1 version which has the similar function with SN74LV1T08DBVRG4?
Thanks