Part Number: SN74LV1T08 Other Parts Discussed in Thread: SN74LVC1G08-Q1 HI BU team
Would you help suggest the part # with Q1 version which has the similar function with SN74LV1T08DBVRG4?
Thanks
Part Number: SN74LV1T08 Hi, Good day. Our customer is using the SN74LV1T08 and they want to know if the below setup will work. in my case, i am giving vcc as 1.8V and for AND gate inputs "one input is 1.8v another is 3.3v" so will it work as expected…
Part Number: SN74LV1T08SN74LV1T08 is an AND gate that is marketed as an excellent level shifter for high frequency and wide voltage range。 I am wondering what is the propagation delay between the input gates? how could we mitigate the delay between input…
Part Number: SN74LV1T08 Hi Sir,
According to the data sheet. there's already a few nano seconds delay to the output.
Is there any chance that I can get a output with 180 degree phase shift?
Thank you.
Part Number: SN74LV1T08 Hello,
I am planning to use part from LV1T logic family (assume PN SN74LV1T08) for my design. I have a condition during which Vcc of the part is not powered but the A and B inputs are getting 3.3V and 5V signals from a different…
Part Number: SN74LV1T08 Other Parts Discussed in Thread: 2N7001T I am looking to use a SN74LV1T08 as a voltage translator between 1.8 V on the input and 3.3 V on the output. It is likely that at some point the input signals will be active while the output…
Part Number: SN74LV1T08 Hi Team,
Linking another thread that I would have replied to in order to not add an additional thread, but it is locked and I am unable to do so. Isn't there supposed to be a new feature to make a new thread based off another…
Part Number: SN74LV1T08 Hi
I am using SN74LV1T08 for reset logic.I am not sure about the input supply voltage that Y i am using this IC.
But I have some doubts:-
1. Is it require pull up resistor at the input side and output side ?
2. I am using…
Part Number: SN74LV1T08 Hi
I am planning to use SN74LV1T08DBVR part for reset logic.
Can i connect the input A and input B at different voltage like input A is at 3.3V and input B is at 1.8 voltage ?
Regards
Nitesh
Other Parts Discussed in Thread: SN74LV1T08 Hello,
Dose SN74LV1T08 arrow to input to Vin(1.8V) before input to Vcc(3.3V).
Our customer worry about reverse current via the protection diode, current sink, etc.
Best Regards.
H.Fujikawa