Part Number: SN74LV1T126 Hi,
We are making a down translation from 5V to 3.3V (powered using 3.3V) for our application. Can we have pull up resistor at the 5V input side
Part Number: SN74LV1T126 Hi All,
I have a question about the SN74LV1T126 datasheet.
There is no description of OP Temp of SN74LV1T126DCKRG4. Please tell me the temperature range.
Best Regards, Ishiwata
Part Number: SN74LV1T126 Hi Team,
Customer wants to double check if below 2 use case are ok?
1) VCC = 1.8V, Input = 3.3V
2) VCC = 3.3V, Input = 1.8V
Thanks!
Andrew
Part Number: SN74LV1T126 Other Parts Discussed in Thread: SN74AUC1G126 Hi, Team
Our customer using our SN74LV1T126 as the Oscillator buffer, they using 2 pcs SN74LV1T126, one is for 3.3V, the other is 1.8V.
the 3.3V device have no problem, but the 1.8V…
Part Number: SN74LV1T126 For this part, can we connect pin A to 5V, Vcc to 5V, but drive the OE pin with 3.3V compatible logic?
We are planning to drive OE pin from 3.3V bank of FPGA.
Output pin we will connect it to 5V logic circuit.
Please check and…
Part Number: SN74LV1T126 We used IC under the following conditions. Why does this IC drop voltage? I thought I would do vCC level OUTPUT. Can you explain the mechanism?
Input : 1.8V
VCC :3.36V
output:約3.12V
Part Number: SN74LV1T126 Hello,
I need help with SN74LV1T126 SPICE Model. I tried to import this file in TINA, but it does not work. During the import process, TINA asked me to choose one of the three components: SN74LV1T126SN74LV1T126_S1 SN74LV1T126_BUF …
Part Number: SN74LV1T126 Hi:
I´m interested to aply a level shifter to a rgb adressable strip control, it has the next atributes and i want to understand better the component to use:
-VCC of 5 Volts
-Vin (data input) 0.7VCC (3.5V minimum ti have…
Part Number: SN74LV1T126 Other Parts Discussed in Thread: SN74AUC1G17 Hi, Team
My customer needs to select a Level Shifter for the clock signal. Clock Fsw=24.768MHz. the signal is unidirectional, and needs to transfer from 3.3V input to 1.8V output. I…
Part Number: SN74LV1T126 Hi Professional,
My customer plan to use SN74LV1T126 and have question for this.
Is this device no problem to apply input signal when this devices power is off?
Best regards,
Kazuki Kuramochi