Part Number: SN74LV244AT Other Parts Discussed in Thread: CD74ACT244 , SN74AHCT244 , SN74AHC573 Hi team,
My customer would like to upgrade their BOM in new project. For below devices, could you please give your suggestions about the P2P replacement part number…
Part Number: SN74LV244AT If VCC is 0VDC, and the inputs to the SN74LV244AT are beginning driven to a TTL high from another active TTL device will the powered off SN74LV244AT input clamp diodes pull DC current and backflow to the VCC of the no powered SN74LV244AT…
Part Number: SN74LV244AT Other Parts Discussed in Thread: SN74ABT126 , SN74LV126A , SN74AHCT126 Hi team,
Could you support selecting logic to meet following customer requirement?
<Customer requirement>
Q. Does TI have SN74LV244ATPW with non-inverting…
Part Number: SN74LV244AT Our customer request us to disclose below information for SN74LV244ATPWR.
*absolute maximum rating for Power dissipation at Ta=85degreeC
*thermal resistance Psi JT
*thermal resistance Theta JC
*thermal resistance Theta CA
Could…
Part Number: SN74LV244AT Other Parts Discussed in Thread: SN74LV245AT Like to use this one but I/O are switched in position. Any other with same functionality exactly that are all inputs on one side and all output are on the other side?
IC: SN74LV244A…
For unidirectional signals, use a unidirection translator like the TXU0104.
For translation from 3.3 V to 5 V, you can also use a buffer with TTL-compatible inputs, e.g., SN74AHCT244/SN74LV244AT/SN74AHCT541/SN74LV541AT.
If "3.3V to 5V" means unidirectional signals, then you can use a buffer with TTL-compatible inputs, such as the SN74LV244AT (or SN74LV541AT with flow-through pinout).
Part Number: SN74AC240 Other Parts Discussed in Thread: SN74LV244AT , , SN74LV541AT , SN74ACT240 Hi team,
Could you recommend what is the best replacement of SN74AC240 with TTL input? I've found SN74LV244AT, SN74LV541AT.
Best regards,
Takeshi Sasaki …