Part Number: SN74LV4052A
This is my schematic using the SN74LV4052ADR. I get a weird DC offset when I force the mux to select channel 3 and send a signal down 2Y3 and measure the output at R67. Which is meesing up the comms such that it doesnt resolve…
Part Number: SN74LV4052A Tool/software: I am currently modelling the parastics of SN74LV4052A. It states the Ron is 25 ohms and Con is 5.6pf.
The datasheet states and Cos (switch terminal capacitance) of 5 pF, Cis (common terminal capacitance) of 23…
Part Number: SN74LV4052A Hi Team,
Posting on behalf of our customer.
I am using SN74LV4052A IC, as UART switching. it's working fine, but there are total 3 variant of the same IC as "SN74LV4052A , SN74LV4052A-Q1 , SN74LV4052A-EP. in SN74LV4052A it…
Part Number: SN74LV4052A Hi,
I have a question regarding the SN74LV4052APWR .
I'm only planning to use 3 out of the 4 available channels . What is the recommended way to handle the unused channel?
Is it acceptable to connect the unused channel…
Part Number: SN74LV4052A Other Parts Discussed in Thread: ADS1118 Hi tech support,
We are designing a multi-channel thermocouple data collector that is used in plastic manufacturing industrial machine. We plan to use 2*SN74LV4502A and 1* ADS1118 to…
Part Number: SN74LV4052A Tool/software: I will do LTspice simulation, so I search the Analog SW products with LTspice parameter.
Vcc under 20V
Please give me the information.
Part Number: SN74LV4052A Tool/software: Hi team, When the voltage of the I/O port exceeds the absolute maximum rating (-0.5V), is the clamp current -20mA? BR, Kengo.
Part Number: SN74LV4052A Tool/software: Hi team
DS shows delay from INH to Y or COM, but customer's design is INH always low, and control by A/B.
Could you please check the enable and disable delay of A/B to Y? Could this delay refer to INH to Y or…
Part Number: SN74LV4052A Tool/software: Hi,
Customer would like to know the SN74LV4052APWR packing (tape and reel) information, since it is not shown in the datasheet.
Can you help to provide?
Or can you check if it would be exactly the same as…