Part Number: SN74LV4T125 Dear TI team,
our company bought SN74LV4T125 kits from mouser, no I am concerning the mark on the top side, which with red highlight on picture underneath, because it not showed in datasheet,
could you please let us know what…
Part Number: SN74LV4T125 Is it acceptable to connect the thermal pad for the RGY package variant of SN74LV4T125 to GND?
It doesn't state in the datasheet what this pin internally connects to, and whether or not it is allowed to be connected to anything…
Part Number: SN74LV4T125 Hi,
I need to test non-shifted signals going through this and hope to not flywire each/unmount this chip. Is it possible to have a 3.3v input to get passed on as a 3.3v output? Currently shifting from 3.3->5v (Vcc).
Thanks…
Part Number: SN74AVC16T245 Other Parts Discussed in Thread: SN74LVC2T45
The VIH of connected device has few margin when I use VCC=3.0V condition, so i would like to check if VOH could be increased when VCC=3.3V is used.
Could you tell me what the VOH…
Part Number: SN74LV4T125 Hi Team,
We understand that VOH is 4.4V(min) at VCC=5.0V, IOH=-16mA.
However, we would like to know Minimum VOH at VCC=5.0V and IOH= less than -16mA (so from 0mA to 15mA).
----------
[Q1]
Could you please let us know if you…
Part Number: SN74LV4T125
Hello, Could you tell me relative propagation delay variation between channels? I want to minimize the delay difference between channels. There is propagation delay spec in the datasheet, but this is part to part variation. I want…
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74LVC3G34 We use the following TI logic IC for driver on the board, And we need to check the minimum and maximum signal propagation delay times for each.
SN74LV4T125RGYR SN74LVC3G34DCUR
=. Request…