Part Number: SN74LV595A-Q1 Tool/software: In the data sheet it doesn't explicitly say for the QFN package whether the exposed pad is connected to GND or left floating.
What is the proper connection?
Part Number: SN74LV595A-Q1 Tool/software: I would like to use the WBQB Packaged version of this IC, however there doesn't seem to be a foot note or mention of how the thermal pad should be connected that I could find in the datasheet (Looking at Rev G…
Part Number: SN74HCS595-Q1 Other Parts Discussed in Thread: SN74LV595A-Q1 , SN74AHC595-Q1 Tool/software: Hello!
What is the rated voltage of the OE pin when VCC is 0V?
Since OE is active low, I plan to pull it up to 5V with 10kΩ outside the IC.…
Part Number: SN74HCS595-Q1 Other Parts Discussed in Thread: SN74LV595A-Q1 , Dear expert,
Customer wants to connect pin SER, Qa~Qh to a connector to connect signal outside of the board. This connector need hot plug. Can our silicon support this?
…
Other Parts Discussed in Thread: OPA890 , CD4066B , SN74LV595A-Q1 , TXB0106 Hello
Could you please recomend a latch or shift register to take and hold data from an MPS430 device sent to the control pins of a CD4066B device? The switch input is a low…
Part Number: SN74HCS595 Other Parts Discussed in Thread: SN74LV595A , Hi team,
Could you give me comment on following customer question? SN74HCS595 and SN74LV595A are candidates for their use case. They consider if those device can be used from serial…
James,
Thanks for your reply. Please see similar question in the Logic Forum "SPI Expander using SN74LV595A". He explains the requirement
for minimum propagation delay and hold time. He also explains how the expander works.
However, he is not intermixing…