Part Number: SN74LV8T245 Hi team,
Could you help provide the amoung weight (mg) info of SN74LV8T245RKSR?
I can't find this info from the Quality, reliability & packaging data website.
www.ti.com/.../report
Regards,
Will
Part Number: SN74LV8T245 Other Parts Discussed in Thread: SN74AHC541 , SN74LV541A Tool/software: Hello. I have a question regarding the SN74LV8T245 octal bus transceiver. We are using this device to translate from +5V (B-side) to +3.3V (A-side) I/O. The…
Part Number: SN74LV8T245 Tool/software: Hi team,
If there is an input to the output pin when Vcc is 0V, the absolute maximum rating says there is no problem, but is there a possibility of backflow to Vcc?
Best Regards, Ryu.
Part Number: SN74LV8T245 Other Parts Discussed in Thread: TXU0104 , TXU0304 hi SIR
Did the SN74LV8T245 is suit for SPI buffer use?
between the FPGA & RF chip , need 133M SPI buffer
thanks
Part Number: SN74LV8T245-Q1 Hi Team,
Customer report that package outline pin order of datasheet page 20 doesn't match pin config in page 3.
This may lead to wrong layout. Please consider to update page 20 pin order.
Thank you!
Marc
Part Number: SN74LV8T245 Other Parts Discussed in Thread: SN74AUC125 , SN74AUC34 I am trying to design a circuit with an SPI interface speed up to 133.33Mbit/s voltage level 1.8V, and a trace length of about 100mm, which also passes by the connector to…
Part Number: SN74LVCC3245A Other Parts Discussed in Thread: SN74LXC8T245 , SN74LV8T245 Tool/software: Hi Team,
Do we have a voltage translator with same package/pinouts as SN74LVCC3245A but 5V side (VCCB side) is TTL compatible?
Thank you!
John
Thank you for your response. I wasn't able to find a datasheet for SN74LV8T245, but I did find one for SN74LVC8T245. It looks like the "LVC" family is a little bit newer, and can be used for faster signals. Is that what you meant?
Thanks again.