Part Number: SN74LVC07A Other Parts Discussed in Thread: SN74LV165A , I'd like to confirm if this design is OK? Are there any points I need to be aware of? Also, the outputs of the SN74LVC07A will connect to pins A-H of the TI SN74LV165A.
Can it be…
Part Number: SN74LVC07A Hi TI team,
We noticed two lots of SN74LVC07APWR (both Malaysia assembly site) show different top marking and internal lead frame (X-Ray) . Would you mind confirming whether both are acceptable?
Sample 1: DC 2606+
Sample…
Part Number: SN74LVC07A Dear Team,
I would like to confirm the output behavior of the SN74LVC07A open-drain buffer under power-off conditions.
Specifically, what will be the state of the output when VCC is not powered (VCC = 0 V or OFF)? Will the…
Part Number: SN74LVC07A Tool/software: Hello support team,
Our customer would like to use the buffer chip for the RJ45's LED (68ohm with 3.3V) to make the blinking signal.
The current consumption would be about 50mA, is SN74LVC07A being suitable here…
Part Number: SN74LVC07A Tool/software:
Hi Sir:
The current test circuit is shown above.
We found that when the input signals at pins 1/3/13 are all pulled high, the measured output signals at pins 2/4/12 are all low.
Why is the measured signal…
Part Number: SN74LVC07A Tool/software: hi
I need a smaller package to replace SN74LVC1G07DCKR/SN74LVC74APWR/SN74LVC126APWR/SN74LVC125APWR. There are many packages on the datasheet. (BQA/RGY). which one is popular? which one is lowest price for selecting…
Part Number: SN74LVC07A Tool/software: Hi,
my customer is looking for soldering profile information for SN74LVC07AD and SN74LVC07ADE4.
I find various documents on ti.com discussing soldering profiles, but I am not sure which one is applicable or how…
Part Number: SN74LVC07A Tool/software: In the circuit given below, the input to the IC is from voltage monitoring circuit. The input to pin 1 is 3.3V and expected output at pin 2 is also 3.3V. Instead the output is 0.4V. What could be the possible reasons…