Part Number: SN74LVC07A Tool/software: Input voltage is normal, no output after access to the circuit, what will cause no output?
The schematic diagram is as follows
Part Number: SN74LVC07A-Q1 Tool/software: Need the confirm AEC standard. As part is Automotive but AEC standard is not mentioned in datasheet.
SN74LVC07AQPWRQ1
Part Number: SN74LVC07A Other Parts Discussed in Thread: SN74LVC1G34 , Customer is looking for 2nd source of this LVC07A. It’s for the gate driver buffer usage and customer hopes driving current is similar existing one. Thanks!
Part Number: SN74LVC07A Other Parts Discussed in Thread: TMP144 , , TXU0204
Hello,
I am working on an application where I plan to interface a TMP144 temperature sensor (which operates at 3.3V logic levels & 5kbps baud rate) with a 5V UART logic field…
Part Number: SN74LVC07A Dear Sir or Madam,
Could you tell me the terminal finish of the part SN74LVC07AIPWREP. Also, could you provide me with thickness of Au in case the terminal finish is NiPdAu or NiAu or Au.
Thanks in advance.
Best Regards,
Kaoutar…
Part Number: SN74LVC07A Hi,
Please tell me TI's point of view about following?
With the circuit configuration as shown in the figure, Even though the input side (pin 11) is HI, the output side (pin 10) is stuck Lo and then toggling the input does not…
Part Number: SN74LVC07A Other Parts Discussed in Thread: SN7417 , SN7407 , TPIC6C595 , TPL7407LA Hi, Support Team
Do we have Similar with SN74LVC07A, but we need open drain output 12v
Typical Vcc is 3.3v
if any suggestion, Please advise me.
Thanks,
Best regards…
Part Number: SN74LVC07ASN74LVC07AD
I ordered qty 40 of this part for a board design. During my test and setup, the chips were not functioning. As in, I connected 5V to Vcc, GND to GND, and 5V to pin 1, 3, and 5 without reading anything on pins 2, 4,…
Part Number: SN74LVC07A Other Parts Discussed in Thread: SN74LVC125A Hi team,
I guess this device is CMOS input.
But in the datasheet, there aren't any specification about the Input transition rise or fall rate Δt/Δv.
Are there any reccomendation…