Part Number: SN74LVC126A Tool/software: To whom it may concern,
I am reaching out on behalf of my employer to request a letter of volatility (LOV) for part SN74LVC126A. The LOV will be used to develop sanitization procedures for hardware which this…
Part Number: SN74LVC126A
Tool/software:
Hi team,
I was referring to the value of 1.65V for VOH and VOL when VCC is 1.8V. However, the SN74LVC126A does not meet the requirement because the minimum value is 1.2V when the required value of the connected…
Part Number: SN74LVC126A Tool/software: Hi,
what is the expected behaviour of the SN74LVC126A outputs in case the supply voltage (VCC) and output enable (OE) are not supplied / low / equal to GND? Thanks in advance.
Best regards,
Jakob
Part Number: SN74LVC126A Tool/software: Is it possible to keep high-impedance in output of 3-state buffers, when the supply voltage is lower than minimum Vcc?
and does that apply to all logic devices specifed by "Partial power down (Ioff)" ?
Part Number: SN74LVC126A Tool/software: Hi team,
My customer plan to use SN74LVC126ADR in their design, they need a datasheet with footprint inside it, but the online datasheet get no footprint info available.
In my hand, I get an previous verion…
Part Number: SN74LVC126A We'd like to use SN74LVC126 3-state Logic to control the transistor (NPN and PNP). As i know, the output of this logic should be push-pull topology, correct? if this is a case, why the IOH (High Level output Current) is negative…
Part Number: SN74LVC126A Hi Team
My customer find it doesn't work when using 6MHz UART data, but It can support 3MHz UART data. I have checked datasheet and it mentioned that SN74LVC126A could support 100MHz application. Can you double check whether…
Part Number: SN74LVC126A Dear Sir:
Regarding the SN74LVC126ARGYR for BT UART application.
Please check the schematic connection whether it is OK and reply us ASAP.
Thanks a lot.
B.R
Vincent
Module
U201 SN74LVC126ARGYR
U201 SN74LVC126ARGYR…
Part Number: SN74LVC126A Other Parts Discussed in Thread: SN74LVC541A In my application there is a case that the outputs of two SN74LVC126As are tied together directly, to drive a common destination. No serial damping resistors are allowed in between…
Part Number: SN74LVC126A Other Parts Discussed in Thread: SN74LV126A Hi Team,
Can you please help us with our customer inquiry below?
My concern is regarding the datasheet for the SN74LVC126A, attached, and how it used in circuit.
In the absolute…