Other Parts Discussed in Thread: SN74LVC157A , SN74LVC1G3157 , SN74LVC541A , SN74HCS365 , TMUX1248 Hi, I have two GPS NMEA standard based. The system that receive GPS data required only one GPS data. The other GPS is for spare purposes. I need to design a simple…
Part Number: SN74LVC157A Good day Colleagues,
Could you help me to find a Tj max (Maximum Junction Temperature) for the SN74LVC157A RGYR device's package?
Thank you in advance, Mikhail
Part Number: SN74LVC157A Other Parts Discussed in Thread: SN74CBTLV16292 , TMUX646 , SN74CBT16232 , SN74CBTLV16211 , TS3A27518E As per the design requirement, 32 digital lines are required to swap the signals. The below Quad part is available but needs to…
Part Number: SN74LVC157A Hi Team,
I have a question about the exposed pad of the mentioned chip.
Shall I connect the EP to GND or leave it floating (connected to the PCB but to no specific signal) please? I cannot find this info in the datasheet.
BR, …
Part Number: SN74LVC157A Hi,
Please provide IBIS model for below part. This part/package is missing in the current IBIS file available in TI website.
SN74LVC157ARGYR
Thanks & Regards
Kranthi
Part Number: SN74LVC157A My question is we use SN74LVC157A and the VCC voltage is 1.8V, what is the MIN Voh when Vcc=1.8V? The test conditions didn’t cover VCC=1.8V situation in the SPEC.
Part Number: SN74LVC157A Hello, I don't understand Luke Sun's answer (Dec 5, 2016 3:18 PM) about 10MHZ SPI with SN74LVC157A.
Dennis said that we can use propagation delay to estimate maximal frequency:
With VCC=3.3V:
2x5.2=10.ns
fmax=1/10.4ns…
Part Number: SN74LVC157A Other Parts Discussed in Thread: SN74AXC1T45 Hi all Would you mind if we ask SN74LVC157A? There is the description "Maximum Output rating VCC+0.5V" on the datasheet. Does "this 0.5V" mean protection diode between output…
Part Number: SN74LVC157A Hi team,
My customer uses the SN74LVC157A to choose the clock source. Because the phase noise is the main concern for the clock, they want to know the isolation of the SN74LVC157A. I don't find the isolation spec of the SN74LVC157A…