Part Number: SN74LVC157A Other Parts Discussed in Thread: SN74LVC1G97 Dear E2E,
Do we have single channel solution whihc is the same function with SN74LVC157A?
BR,
Jason
Part Number: SN74LVC157A Hi, Team:
My customer want to know if the SN74LVC157ADR VCC is off, but the IO still have input voltage, such as 3.3V, do the SN74LVC157ADR is ok with this voltage and have no impact on the chip's reliabiity?
Thanks!
2× SN74LVC157A, or SN74AHC157 with lower drive strength.
You could also use a single buffered or analog multiplexer (SN74LVC1G97 or SN74LVC1G3157) to drive eight buffers (SN74LVC541A or SN74AHC541).
Part Number: SN74LVC157A Other Parts Discussed in Thread: SN74LVC257A Team,
Can you please help in crossing the NC7SZ157P6X ROHS?
Please provide me with the exact part number and not just GPN.
Please let me know
Thanks
Part Number: SN74LVC157A Other Parts Discussed in Thread: SN74AHC157 , , CD74HC157 Hello team,
My customer want to find 2nd source of SN74LVC157ARGYR, except this part, do we have p2p part to suggest? My customer can choose two parts from one chip vendor…
Other Parts Discussed in Thread: SN74LVC157A Hi team,
What's the max signal rate of SN74LVC157A in 3.3 or 1.8V application?
Customer wants to evaluate whether it could be used in a 10MHz SPI bus (1.8V/3.3V).
Thank you!
Part Number: SN74LVC157A Hello team,
My customer use SN74LVC157A, and they test waveform of pin1and find Input transition rise or fall rate is 82ns/V, which is much higher than our spec 10ns/V, they want to know if this applicatioin is OK, it is risk…
What is the clock frequency?
As far as I can see, the SDOUT signal does not need muxing.
LVC devices have overvoltage-tolerant inputs, so you can simply run a multiplexer like the SN74LVC157A at 1.8 V. To translate SDOUT, use the 2N7001T or SN74AXC1T45…
Sorry, I was mistaken. The turn-on/turn-off times are not related to the frequency of the PWM signal that can be passed through the switch. What matters is only the bandwidth. All four switches mentioned above have a bandwidth high enough to allow a 20…