Part Number: SN74LVC16T245 Hello,
The following circuit has the path from C1 to J1 as a multi-layer flex circuit. Assume the flex has been damaged with possible shorts. C1 is not accessible. Readings can be taken only from the J1 side.
Is it possible…
Part Number: SN74LVC16T245 Other Parts Discussed in Thread: 74ACT16861 , SN74ABTH32245 Hi, we need to choose a 3.3-V to 5-V Level-Shifting Transceiver, and we are considering SN74LVC16T245, but the bits of this one are only 16, if there are any other T…
Part Number: SN74LVC16T245 Hi Team,
According to the page 7 of the datasheet, the threshold voltage is stated to be determined by the value of VCCI. When VCCI = 1.65V to 1.95V, 4.5V to 5.5V, it seems to change with VCCI. When VCCI = 2.3V to 2.7V, 3.0V…
Part Number: SN74LVC16T245 Other Parts Discussed in Thread: SN74LVCH16T245
Hello,
After reading more about this part from the datasheet and this application note, I have a few clarifying questions. http://www.ti.com/lit/an/slva746/slva746.pdf
First here…
Part Number: SN74LVC16T245 Dear all,
one of my AA is using the SN74LVC16T245 to level shift data and clock signals from VccA=3.3V to VccB=1.8V.
The clock and data have to run at 16MHz, so the skew is important to understand if the clock and data remain…
Part Number: SN74LVC16T245 Other Parts Discussed in Thread: SN74AXC8T245 Hello,
1. Assuming this device acts as a level translator between an FPGA (3.3V) and C6654 DSP (1.8), what is the estimated current per I/O and power drawn by the device? Ballpark…
Part Number: SN74LVC16T245-EP Other Parts Discussed in Thread: SN74LVC16T245 TI provides IBIS model for SN74LVC16T245 but i am using SN74LVC16T245-EP, so are these IBIS models are same or is there any difference.
Part Number: SN74LVC16T245-EP Hello,
I am using a bidirectional Level translator SN74LVC16T245-EP in one of our project. I have confusion that How should be OE pin before VCCA and VCCB are fully ramped and stable?
Any special power supply recommendation…