Part Number: SN74LVC16T245-EP Tool/software: Hi Sir,
I am using "CLVC16T245MDGGREP" from the "SN74LVC16T245-EP" family
I have activated enable and direction pins but am not giving any inputs to input pins (For Eg-1A1) it is in a high…
Part Number: SN74LVC16T245-EP Hi,
We wanted to know the maximum input voltage of SN74LVC16T245-EP. We are having confusion regarding the spec VI/O Input/output voltage given in the datasheet.
The use case is to supply 3.3V input to the transceiver powered…
Part Number: SN74LVC16T245-EP Hello TI,
I have some question about partial power down and vcc isolation feature
Q1: I'm planning to use translator in a system with two different voltage levels.
Vcca will always be active. Vccb will turn on and off…
Part Number: SN74LVC16T245-EP Other Parts Discussed in Thread: SN74AVCB164245-EP
Hi Team,
would like to use the sn74lvc16t245-ep to perform voltage translation on a clock running at 16MHz along with the data clocked by this clock. Is this part suitable…
Part Number: SN74LVC16T245-EP Team,
My customer has the following question: I guess that the part that I am not clear on is that where in the datasheet are these parameters that are mentioned below? I would expect to see jitter, skew, rise time / fall…
Part Number: SN74LVC16T245-EP Hi Team,
My customer would like to know if the SN74LVC16T245-EP is suitable for data rates of at least 50MHz?
Thanks, Mitchell
Part Number: SN74LVC16T245-EP Hi All,
In my Project I am using one 16 bit level translator SN74LVC16T245MPWREP, one 8 bit level translator SN74LVC8T245MPWREP, one 2 bit level translator SN74LVC2T45MDCTTEP in which signals are connected to a Micro D connector…
Part Number: SN74LVC16T245-EP Dear Sir,
We are planning to use SN74LVC16T245-EP in our existing design.
In view of the above we want to know the end of life of the product.
Regards, Arun P
Part Number: SN74LVC16T245-EP Hi,
I am using a bidirectional level translator (P/N CLVC16T245MDGGEP) from SN74LVC16T245-EP series.
Do I need to hold the OE# pin in any recommended logic level until VCCA and VCCB are fully ramped & stable?