Part Number: SN74LVC1G00 Tool/software: Hi Team,
What is the VOH and VOL levels when VDD=3.3V and VDD=5V??
There is no detail given in datasheet.
Regards,
Vidhya
Part Number: SN74LVC1G00 Other Parts Discussed in Thread: LM339 , SN74LVC00A , SN74HCS00 , SN74LVC1G10 Hello,
hoping to get some input on my design,
I want to latch some LM339 comparator output (active low) for overcurrent and ground fault, and i wish to…
Part Number: SN74LVC1G00 Hi There,
I am using SN74LVC1G00, but it broke down at my business partner. Upon investigation, the output terminal was found to be short-circuited. (about 3Ω) I believe that the internal nMOS was shorted due to overvoltage…
Part Number: SN74LVC1G00 Hi
I'm looking for series of SN74LVC1G(withoutR) for our product, but my supplier offred me parts number which has R.
Please let me confirm the difference of part numbers which are with R and without R .
SN74LVC1G07DCK R
SN…
Part Number: SN74LVC1G00 Hi support team.
Our customer needs the Ibis model for DRL(SOT-5X3) package.
Is it possible that you provide the Ibis model for DRL( SOT-5X3 ) package?
Best regards,
Higa
Hi JP,
Here is the data:
Result- Theta JA-High K (standard datasheet value)
235.6
Result-Theta JC, top (standard datasheet value)
151.3
Result-Theta JB (standard datasheet value)
121.6
Result- Psi JT (standard datasheet value)
43.7
Result-…
Part Number: SN74LVC1G00 Typically pullup resistor values for logic inputs are in the range of 4.7K ohm to 10K ohm.
However, there are some situations where I would like to use a higher value.
This is usually to save power, or when the driving device…
Part Number: SN74LVC1G00
Please provide the maximum reflow temperature and the time associated with maximum reflow temperature(tp) for SN74LVC1G00DCKR. Please refer to the below image.