Part Number: SN74LVC1G08-Q1 Tool/software: Hi,
in the functional safety document for this part, there is only failure rate and failure mode distribution information. For our safety analysis we need a pin FMEA for every IC. Is there additional information…
Part Number: SN74LVC1G08-Q1 Tool/software: Hi all,
The datasheet for SN74LVC1G08-Q1 mentions "It can produce 24 mA of drive current at 3.3 V".
It also mentions a 50 mA maximum rating for I O.
I assume that the drive capability is a result …
Part Number: SN74LVC1G08-Q1 Other Parts Discussed in Thread: SN74LVC1G99-Q1 Tool/software: Hi,
What is the state of input/output pin when VCC is under voltage?
Part Number: SN74LVC1G08-Q1
Hi Team,
do we have any better alternative in the meanwhile for 74LVC1G08GW-Q100?
https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1044999/sn74lvc1g08-q1-sn74lvc1g08dckrq1-to-beat-74lvc1g08gw-q100?keyMatch=74LV…
Part Number: SN74LVC1G08-Q1 Other Parts Discussed in Thread: SN74LVC1G08 Hello Logic Team,
can you provide a Spice model of SN74LVC1G08? Preferred unencrypted model.
Thanks and best regards,
Michael
Part Number: SN74LVC1G08-Q1 A customer is concerned that the initial automotive qualification data for SN74LVC1G04QDCKRQ1 from 2015 does not meet current automotive standards. Is there another device that we qualified by similarity for technology to this…
Part Number: SN74LVC1G08-Q1 Hi Expert
My customer use case as below:
pin1 always =5V(Pin1 connect to VCC)
Pin 2 normally is float and triggered low voltage when system fault.
Y connect 3.3V voltage that normally current is limit 100mA.
when Pin2 tie to…