Part Number: SN74LVC1G11-EP Hi,
I am using SN74LVC1G11MDCKREP gate in my design. I need junction to case resistance information for the IC.
From datasheet I got junction to ambient resistance. Is there any information available on thermal resistance for…
Part Number: SN74LVC1G11SN74LVC1G11DCKRG4 , which the size and orientation of die and pins seems different. Please review to see if both variants of the IC are correct and can be used. Thanks
Thanks
Calvin
Part Number: SN74LVC1G11 Hi team,
My customer want to know if the SN74LVC1G11 could replace the Nexperia 74LVC1G11GW . (Pin to Pin and Bom to Bom)
Can team help me to check again. I need to make sure if it is ok to replace it.
Part Number: SN74LVC1G11-EP Other Parts Discussed in Thread: SN74LVC1G11 Hello Guys,
Good day.
Do we have PSpice model for SN74LVC1G11MDCKREP?
I found that the non-EP version SN74LVC1G11, has both IBIS and Behavioral Spice model. Can they use this instead…
Part Number: SN74LVC1G11 HI Team,
I am using SN74LVC1G11DBVR.
1.Input current limit per pin (A.B.C pins) is 5uA?
2. If the logic high input that I am driving is in mA, should I limit this current using a series resistor?
But IIK limit is 50mA.
3. Can this…
Part Number: SN74LVC1G11-Q1 Hi expert,
SN74LVC1G11-Q1 is a device that named with Q1, but in datasheet i don't find AEC-100 certification. And the operating temperature is -40-85C. For automotive application, it always need -40-125C. Could you confirm…
Part Number: SN74LVC1G11 HI,
SN74LVC1G11DCKRG4
The size and orientation of the die for the sample of DC: 2117 is different to that of the other two (2) samples. samples failed the Solderability Test.
die for DC: 2117 is different from the die of the…
Part Number: SN74LVC1G11 Other Parts Discussed in Thread: SN74AHCT1G125 , SN74AHC125 Hi team,
My customer want to use SN74LVC1G11 in their design and have some questions as below, could you please help to check and provide some advice?
Thanks!
If VCC…
Part Number: SN74LVC1G11-Q1 Other Parts Discussed in Thread: SN74LVC1G11 Hi,
SN74LVC1G11
Does this device accept 5V inputs when it is powered by 3V3 supply.
Regards
Siva