Part Number: SN74LVC1G11-EP Hi Team,
I am looking to use the SN74LVC1G11-EP as a driver for a PWM DAC and am wondering if there is any additional info on the voltage drop and rise above ground when the part is sourcing and sinking current respectively…
Part Number: SN74LVC1G11-EP Hi,
I am using SN74LVC1G11MDCKREP gate in my design. I need junction to case resistance information for the IC.
From datasheet I got junction to ambient resistance. Is there any information available on thermal resistance for…
Part Number: SN74LVC1G11-EP Other Parts Discussed in Thread: SN74LVC1G11 Hello Guys,
Good day.
Do we have PSpice model for SN74LVC1G11MDCKREP?
I found that the non-EP version SN74LVC1G11, has both IBIS and Behavioral Spice model. Can they use this instead…
Part Number: SN74LVC1G11-EP Hello,
We are using SINGLE 3-INPUT POSITIVE AND GATE SN74LVC1G11-EP. And we need to ensure that its output stays at 0 during power up and power down.
During power up, can the output be momentarily driven high by the IC ? Up…
Part Number: SN74LVC1G11-EP Hi Team,
Our customer is looking for the junction-to-case thermal resistance of SN74LVC1G11MDCKREP.
Thanks!
Best regards,
Carl Ramirez
Part Number: SN74LVC1G11-EP Hi,
I have some questions regarding the protection circuit (if there are any) for the little logic family:
Question 1: Are there input protection diodes integrated in the SN74LVC components, to DGND and to VCC ?
Question 2…
Part Number: SN74LVC1G11-EP Hi again,
I have some follow up questions on this part.
Here they are:
What is the detailed over voltage protection mechanism ?
Does this protection limit both the input current and the input voltage ? How ?
We may have continuous…
Part Number: SN74LVC1G11-EP Hello ,
I am using SN74LVC1G11-EP component, my VCC voltage is 5V .
according to datasheet the VOH MIN is 3.8V and it ok with my design .
but the VIH MIN is 0.7*VCC it means 0.7*5V=3.5V .
if my inputs are working with 3.3V and 3V…
Part Number: SN74LVC1G11-EP Hi Sir,
We saw orderable P/N SN74LVC1G11DCKREP on datasheet, page 1.
But it shows the orderable device is SN74LVC1G11MDCKREP on datasheet page 6, is it the same ? or the mistake ?
pls confirm.
thanks.
Mac.
Part Number: SN74LVC1G11-EP Our certificate of conformance identified the date code as 72MC32E. The part packaging is marked as 1706+5. Can you provide the document needed to translate the 72MC32E to the date code on the packaging?
Thanks, Carolyn Sl…