Part Number: SN74LVC1G123 The datasheet mentions "Glitch-Free Power-Up Reset on Outputs", but I'm not finding a definition for this.
Our design holds !A low. B, !CLR, and VCC all come up together. We're seeing inconsistent behavior at power-up (sometime…
Part Number: SN74LVC1G123 HI,
Is the below diagram correctly interpreted ?
If R L and C L are involved in the calculation, how does the calculation?
If t w = K x C ext x R ext = 1.11 x 28pF x 2kohm = ~62ns . It is not match with the reading…
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: SN74HCS72 Hi team,
My customer is considering the circuit which turns off LED driving FET if the FET gate pulse lengh is longer than specific length (a couple of mill seconds).
Is SN74LVC1G123…
Part Number: SN74LVC1G123 Dear team,
Could you kindly share the equivalent circuit at 7 pin to make sure whether there is protection circuit or not ?
Our customer would like to make sure it.
Your understanding would be highly appreciated.
…
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: SN74LV221A I have a puzzling case of a not so rare failure of the SN74LVC1G123DCTR part in production. I am seeing occasional (perhaps 1 in 500) failures of the SN74LVC1G123DCTR to function correctly…
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: SN74LV221A-Q1 , SN74LV123A-Q1
Hi Team.
Customer asks if sn74lvc1g123 is available for automotive Qualify.
Is sn74lvc1g123 available for automotive Qualify?
Or is there an alternate product…
Part Number: SN74LVC1G123 Hi
Some similar devices directs that Cext pin should be tied to GND but our SN74LVC1G123 does not.
Why doesn’t it need to be tied to GND for SN74LVC1G123?
Thank you and best regards,
Michiaki
Part Number: SN74LVC1G123 Its datasheet shows (below table) that with a 10kOhm resistor and a 0.1uF Capacitor at Vcc=1.8V, the pulse width is typically 1ms and max 1.1ms over the -40~+85C temp range.
My question now is: what is the minimum pulse duration…
Part Number: SN74LVC1G123 Dear *,
we want to give a LED a fade-out is the SN74LVC1G123 a good choice?
optoelectronics.liteon.com/.../LTST-C191TBKT.PDF
Can we direct drive the led from the output of SN74LVC1G123? or do we need a mosfet?
Is…
Part Number: SN74LVC1G123 Dear sir,
Our customer is using SN74LVC1G123, and below is the schematic:
Ideally, the output Q (pin5) should change form Low to High and produce a pulse when the input A (pin1) in the transition from High to Low, right…