Part Number: SN74LVC1G123 Hello
There is a YZP package drawing in "5 Pin Configuration and Functions" in the data sheet, and pin numbers 1 to 8 are assigned. On the other hand, there is YZP0008 PACKAGE OUTLINE on page 23 of the data sheet, and pin numbers…
Part Number: SN74LVC1G123 Hi
Could you provide the data of pulse width variation over temperature ?
I found the application report SLVA720 which shows the variation between 10℃ - 85℃ but customer needs the data over temperature.
Thank you and…
Part Number: SN74LVC1G123 I have a problem when using TI's sn74lvc1g123. Please help me analyze it. The following picture is the circuit. Input gives a rising edge, and output output will maintain a level of about 0.9V instead of a pulse. Please help…
Part Number: SN74LVC1G123 hello all,
I would like to confirm what is the Icc quiscent when Vcc is 3.3V. customer measure the quiscent on Icc but it shows 2uA. is it reasonable ? Will we define it at datasheet ?
Part Number: SN74LVC1G123 Hello,
I want to generate a pulse of about 1s with SN74LVC1G123.
(Outside the range of Figure 4 in the data sheet) Can I use the following formula for calculating the pulse width? tw = K × τ = K × R × C (K = 1)
Best re…
Part Number: SN74LVC1G123 Hi,
1)I would like to the minimum output pulse width that can be obtained from this device.
2) Is it possible to get pulse width of 5ns,if so what are the values of Rext and Cext that i should choose
Thanks
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: ISO7810 , STRIKE
Hi,
I'm currently having a problem using SN74LVC1G123 -- the output pulse isn't appearing. An image of it in my schematic can be seen below. I would like it to trigger on…
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: TLV840 , LM555 Hi Team,
Our customer is looking for a device that would generate an automatic pulse of 1 second after the board has been powered on. The device will remain off after the pulse…
Part Number: SN74LVC1G123 hi
For the "minimum retrigger time" on the other hand, no value is to be determined from the existing diagram because Here the parameter value C = 100nF has not taken into account - and, incidentally, no resistance value is…
Part Number: SN74LVC1G123 Hi,
Could you please kindly suggest the Icc of SN74LVC1G123 at Vcc=3.3V?
Since the datasheet only shows the Icc=20uA at Vcc=5.5V but no data at 3.3V.
Thanks a lot for your support!