Part Number: SN74LVC1G123 Hi,
Could you please kindly suggest the Icc of SN74LVC1G123 at Vcc=3.3V?
Since the datasheet only shows the Icc=20uA at Vcc=5.5V but no data at 3.3V.
Thanks a lot for your support!
Part Number: SN74LVC1G123 Hello Experts, I would like to know how to decide "K" value when it is case which is not a range in datasheet. I would like to design 30s duration by SN74LVC1G123. The datasheet stated max 0.2s. (R=200Kohm, C=1uF at VCC=5V, Figure…
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: SN74LVC1G17 Hi,
My customer is using LTC6994 for ~2mS delay block (i.e. output 50% duty cycle pulses are delayed by ~2mS wrt input pulses).
Can SN74LVC1G123 be used for same ?
What is expected…
Part Number: SN74LVC1G123 Hi Team,
I have a question about SN74LVC1G123 Rext/Cext pin abso max spec.
Datasheet doesn't describe Rext/Cext pin I/O information so I don't know its V_Rext/Cext abso max spec.
Could you let me know Rext/Cext pin…
Part Number: SN74LVC1G123 Dear Specialists,
My customer'd like to adopt SN74LVC1G123 and has a question.
I would be grateful if you could advise.
---
What is the latch-up immunity current?
Generally, it is specified JESD78 as 100mA.
is this…
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: SN74LV123A Hi, team.
If the Cext of SN74LVC1G123 is large, is a protection diode necessary? In the case of SN74LV123A, there are the following descriptions, but there is no description in SN74LVC1G123…
Part Number: SN74LVC1G123 Hi,
Is the duration decide by PR602 and PC600?
In this application the Q duration should be 2580ms, am I right?
Is there exist any limitation for R and C or Q’s pulse time?
Best regards,
Randy Chen
Hey Troy,
There's an FAQ on this topic:
I know it's probably not the answer your wanted to hear though. Please let me know if I can be of further assistance.
Hi Marcos,
Since you are internal to us, please go to your TI web browser and type " modelrequest/ "
If you don't have the confluence ID, please register and there is a chance you have to wait up to 1 hour for first time user activation.
Herma…
Part Number: SN74LVC1G123 Team,
My customer is looking at using the SN74LVC1G123 (multivibrator) in a ~200-300 ns pulse width application.
Figure 4 indicates that RL of 1k and Cext of 100pF could yield about the correct pulse width.
…