Part Number: SN74LVC1G123
[Case:710338]Technical Data Inquiry
SiliconExpert is contracted by our customer to work with their suppliers for accuracy and compliance purposes.
The part "SN74LVC1G123-DCU" was Active based on the email " ">download…
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: TPL5110 hello ti,
we want to program output pulse width of approx 10 seconds,
is SN74LVC1G123 is able to generate this much duration pulse.,
looking at the datasheet , the maximum duration shown…
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: BQ25121A , Hi,
I have an application where an external switch is continuously pressed when in operation and released when not. It is powered by a battery which in turn is controlled by a BQ25121A…
Part Number: SN74LVC1G123 Hi Team,
I want to use this IC in my design to latch an interrupt for 1 second.
The input voltage is 1.8V (and so is the interrupt nominal voltage), and the capacitance graph only goes to 10^6 pF.
I want to use R_L of 200kOhm…
Part Number: SN74LVC1G123 The pinout of the YZP part on p. 3 of the data sheet is numbered 1 to 8, which is not typical for a BGA. The pin numbers on the footprint and package drawings (p. 24-27) are numbered as usual for BGA.
Please confirm that pin…
Part Number: SN74LVC1G123 Hi Everyone,
I need to know the reference levels tolerance of the Cext/Rext pin which trigger the output to high or low.
I want to make a precise pulses (500ns +- 20ns of tolerance) and I need to know how precise those reference…
Other Parts Discussed in Thread: SN74LV221A , SN74LVC1G123 , SN74LV123A Hi,
I was wondering why there is a model of the SN74LVC1G123 / SN74LV123A but none of the SN74LV221A? I found this thread "e2e.ti.com/.../faq-why-is-there-no-pspice-model-for-a-monostable…
Part Number: SN74LVC1G123
Dear Suport,
Why SN74LVC1G123DCUR got top ic marking C23J but SN74LVC1G123DCUT dont have? Isn't that both are the same part except package order quantity?
Any mistake on the datasheet.
Best Rgds,
Felix
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: TIDA-060008 Should CEXT (pin 6) be connected to GND? In the TIDA-060008 it is connected to GND but the datasheet is only to one of the capacitor ends.
Part Number: SN74LVC1G123 Other Parts Discussed in Thread: SN74LVC244A I want to generate a pulse that always falls between 20ns and 50ns over the entire temperature range of an industrial device. Is 20ns a feasible lower bound for this device? I have…