Part Number: SN74LVC1G125-Q1 Hello,
The available SPICE model not working in HyperLynx. Can you able to share generic SPICE model or IBIS model?
Thanks,
Manikandan M
Part Number: SN74LVC1G125-Q1 Tool/software: Hello -
(2) Questions.
1. After scanning the "SN74LVC1G125-Q1 Single-BUS buffer gate with 3-state output" datasheet which contains the part number in question "1P1G125QDCKRQ1." Sheet 14 (Packaging Information…
Part Number: SN74LVC1G125-Q1 Hello Ti engineers,
there is a SN74LVC1G125-Q1 in our design,the OE is tie to GND ,and A is from outside device (SPI_MISO) , and Y connect to MCU ,we found that when A is tristate,Y is low,but MCU cannot control the AURIX_SPI3_MISO_3V3…
Part Number: SN74LVC1G125-Q1 Hi,
customer need the failure rate to classify it in SN29500-2.
Which Table and Category of SN29500-2 is it?
Regards, Holger
Part Number: SN74LVC1G125-Q1 Hello customer,
My customer is using this device as below.
If the power sequence of PP3V3_MISC1 is early than VCC PP1V8_AO, is there any risk that will lead to the IC damage? If there any risk to lead the IC behave abnormal…
Part Number: SN74LVC1G125-Q1 Hi team,
Customer needs to use SN74LVC1G125-Q1 in sleep mode and cares about the Icc current at different cases. Could you pls share input Icc current for below scenario?
OE
IC output status
Load
…
Part Number: SN74LVC1G125-Q1 Other Parts Discussed in Thread: PCA9306 Hello TI engineer,
In our design ,we use SN74LVC1G125-Q1 as buffer for SMI bus,i want to know if i can use PCA9306DCUR(an level -shift device) to replace SN74LVC1G125-Q1. Are there…
Part Number: SN74LVC1G125-Q1 Hi,
Can you remind us of the reason there are two currents specified for Vcc of 3V in table 6.3 for I OH and I OL ?
Thanks,
HSG