Part Number: SN74LVC1G126-EP Other Parts Discussed in Thread: SN74LVC1G126B-Q1 , A part in the same family, the SN74LVC1G126B-Q1 is AEQ certified and has the temperature limits of -40°C to +125°C. The SN74LVC1G126-EP part is an enhanced product but only…
Other Parts Discussed in Thread: SN74LVC2G34-EP , SN74LVC1G126-Q1 , SN74LVC1G126
Hello,
If an output from SN74LVC2G34-EP or SN74LVC1G126-Q1 is pulled up to 3.3V through a 10kohm resistor while the device is unpowered, is that okay? Or could it damage…
Part Number: SN6505B Tool/software: Hi Team,
Can SN6505B meet the NBIOT Module conditions?
• VINP = 5.5V:
When the ambient temperature is -40°C, the maximum output current is about 170 mA
When the ambient temperature is 25°C, the maximum output…
Hi Jim,
The Fs value of 1000Msps with JMODE0 was selected at the GUI; so for both channels of the ADC, the JESD protocol uses the first four lanes, which are connected to the transceiver pins of the FMC connector. The signal to be sampled was 100mVpp…
a10_soc_devkit_03_31_2016.pdf Thanks JIM
Pls confirm whether u have checked with "DK-DEV-1SGX-L-0A" or "DK-SOC-10AS066S-A" just in case i am attaching the scematic of "DK-SOC-10AS066S-A". Kindly look at the FMC site A & B whichever is suitable.
you…