Part Number: SN74LVC1G3157-Q1 Other Parts Discussed in Thread: SN74LVC1G3157 Hi TI Team,
I'm using SN74LVC1G3157 for generating Reset Signal for my MCU based on input signals (B1,B2 & S).
My B2 Signal is continuously pulled high to 1.8V, have connected…
Part Number: SN74LVC1G3157-Q1 Other Parts Discussed in Thread: SN74LVC1G3157 Hi team,
I found a change in absolute max rating value of Select pin (VIN) and VI/O pin in the datasheet.
Could you please double check if this change is correct?
December…
Part Number: SN74LVC1G3157-Q1 Hi team,
Would you pls help share how to evaluate the power dissipation and thermal performance of SN74LVC1G3157-Q1 under below condition? Customer is concerning since our thermal resistance on datasheet is large.
Supply…
Part Number: SN74LVC1G3157-Q1 Hello Experts, My customer would like to know a power consumption at Ta=105degC. Do you have such data? Best Regards, Fujiwara
Part Number: SN74LVC1G3157-Q1 dear
Does this index require the slope of the control signal s, or the slope of the transmitted signal B 1/B 2 and A which show as below? thanks in advance
Part Number: SN74LVC1G3157-Q1 Hello,
Can you please provide details on the what the impedance of pin A (4-common terminal) is when the device is powered off and if this pin as internal protection diodes that are connected to VCC?
Thank you,
A…
Part Number: SN74LVC1G3157-Q1 Hello, Team,
Customer is using the device with Vcc = ~5V for the normal operation.
They would like to know whether if the Vcc drops to 4V, would SW still function? Are there any modes that needs to be taken into consideration…
Part Number: SN74LVC1G3157-Q1 Hello,
Good Day!!
We would like to use the component 1P1G3157QDBVRQ1 for our upcoming design, hence please share the life cycle (EOL) of it.
As per our requirement, the component should have EOL of at least 15.…
Part Number: SN74LVC1G3157-Q1
Hello, team,
Customer is currently investigating their issue and would like to know the effect of analog-switch being latched-up. This is needed because they want to narrow down the causes of this issue.
For example…