Part Number: SN74LVC1G32 Hi Expert,
I find a strange things in SN74LVC1G32 and SN74LVC1G32-Q1 datasheet. I suppose these two are only different for auto version. As for package, they should be in the same size. But I find they have different size even…
Part Number: SN74LVC1G32 Other Parts Discussed in Thread: SN74LVC1G97 Hi Sir,
With SSD application, SN74LVC1G32 is applied on power disable function. we'd like to debounce time of input signal.For example, <1us signal drop would not trigger SN74LVC1G32…
Part Number: SN74LVC1G32 Other Parts Discussed in Thread: SN74LVC1G07 Hi TI Team,
I have one doubt regarding SN74LVC1G32QDCKRQ1 OR Gate IC.
If i am connecting this IC VCC Pin 5V and and IC out put side pin we connected 1K resistor through 6.5V for other…
Part Number: SN74LVC1G32 Hi Team,
Please help to check does SN74LVC1G32DSF2 fully same with SN74LVC1G32DSFR?
Only different on Pin1 Quadrant ?
Thanks!
Kai
Part Number: SN74LVC1G32 What is the difference between SN74LVC1G32DSF R and SN74LVC1G32DSF 2 ? I show the lead finish is different between the 2 but both are 5K reels. Does this means there are 2 different build locations? Is there a performance difference…
Part Number: SN74LVC1G32-EP Other Parts Discussed in Thread: SN54AC14-SP , SN54AC00-DIE , SN54AC00-SP , SN54AC02-SP , SN54AC02-DIE , SN54LVC646A-SP Dear TI Team,
Is there any report/document that contains single event effects information for SN74LVC1G32-EP…
Part Number: SN74LVC1G32 Hi TI Team,
I have the device SN74LVC1G32DCKR with a date code 2113 on the label.
However, the binary code marked on the unit is with DC 2114-2117.
May I know why the DC on label is different from actual DC marked? Any reason…
Part Number: SN74LVC1G32 Hi,
I'm using SN74LVC1G32YZPR (DSBGA (YZP))
and checked pin assignment in datasheet and land pattern in Ultra Librarian.
It seems the assignment is different.
for example,
pin C1 is "GND" in the datasheet
but pin…
Part Number: SN74LVC1G32 Hello Expert,
Can you help to check if we has a pin to pin part but with a invert input of this OR gate as below? SN74LVC1G32DBVR
Appreciate your support.
Thanks!
Jim
Part Number: SN74LVC1G32-Q1 Hi Sir,
I am looking for pin to pin replacement of NLVVHC1GT32DFT1G, I found SN74LVC1G32QDCKRQ1.
Is this part automotive qualified? I can not find "AEC-Q100" or even "automotive qualified" wording in datasheet.…