Part Number: SN74LVC1G32 Hi,
I'm using SN74LVC1G32YZPR (DSBGA (YZP))
and checked pin assignment in datasheet and land pattern in Ultra Librarian.
It seems the assignment is different.
for example,
pin C1 is "GND" in the datasheet
but pin…
Part Number: SN74LVC1G32 Hello Expert,
Can you help to check if we has a pin to pin part but with a invert input of this OR gate as below? SN74LVC1G32DBVR
Appreciate your support.
Thanks!
Jim
Part Number: SN74LVC1G32-Q1 Hi Sir,
I am looking for pin to pin replacement of NLVVHC1GT32DFT1G, I found SN74LVC1G32QDCKRQ1.
Is this part automotive qualified? I can not find "AEC-Q100" or even "automotive qualified" wording in datasheet.…
Part Number: SN74LVC1G32 Hi Expert,
My customer would like to replace SN74LVC1G32DSFR with SN74LVC1G32DSF2.
1. Does it have any concern if directly change?
2. I checked datasheet and found that they use differential lead finish. What is the advantage and…
Part Number: SN74LVC1G32 Kindly review the attached schematics designed using SN74LVC1G32DCK3 . Input signal is from processor and output is connected to display.
Please review the design and kindly let me know your comments.
Part Number: SN74LVC1G32 Hi team,
My customer uses SN74LVC1G32DRYR, in 95~100℃ temperature range, when VCC goes from 3.3V to below 1.65V, the output will go from 0 to the voltage equal to VCC and follows VCC(which is below 1.65V now). Is it a normal behave…
Part Number: SN74LVC1G32-Q1 Other Parts Discussed in Thread: SN74LVC1G08-Q1 Hello,
Kindly review the attached design using SN74LVC1G32QDBVRQ1 Thanks,
Melbin
SN74LVC1G32QDBVRQ1_SCH_28DEC2020.pdf
Part Number: SN74LVC1G32 Hi expert,
I have 2 questions about the device.
1. Min Supply voltage, "Data retention only is 1.5V" in the datasheet, means that the minimum voltage that can maintain the output state is 1.5V? If supply is lower than this voltage…
Part Number: SN74LVC1G32 Other Parts Discussed in Thread: SN74AHCT1G32 Hi TI
There are tow questions that need to confirm.
1.When Vcc is 5V, the threshold is Vcc×0.7 or V M (Vcc/2) ?
If the input voltage is 3V, can it operate normally?
2.And why…
Part Number: SN74LVC1G32 Hello expert,
May I know what is output level when input is floating? After checking with FAQ question 1, it seems like floating input will get unknown level for output. May I know if we need to pull input to low with large resistor…