Part Number: SN74LVC1G373 Hello,
On the SN74LVC1G373, the datasheet indicates that the output can be driven with a negative voltage provided that the current is limited to 50 mA.
What about for voltages above Vcc?
If a level was presented to the output…
Part Number: SN74LVC1G373 Other Parts Discussed in Thread: SN74LVC1G34 Hi,
DO we have PSPICE Model for SN74LVC1G373DBVR?
Hope for sharing. Thanks a lot.
Part Number: SN74LVC1G373 Hi team,
Is there any difference between SN74LVC1G373DCKR and 74LVC1G373DCKRG4?
I do understand more or less G4 suffix, but what is the meaning of SN prefix?
According to datasheet the difference in Lead finish/Ball material.…
Part Number: SN74LVC1G373 Hi team,
The customer want to use single channel D latches with automotive grade. Do we have such device?
最小供电电压[VDD(Min.)]
1.65V
最大供电电压[VDD(Max.)]
5.5 V
三态输出[Tristate Output]
Yes
最大位宽[Data Bus Width (Max.)]
\
最大工作频率…
Part Number: SN74LVC1G373 Other Parts Discussed in Thread: SN74LVC1G175 , SN74HCS74 Hello,
How can I perform the 74LVC1G373 or other suitable device as a clocked latch as LE behave more like a pass throuh must support low current consumption.
required functionality…
Part Number: SN74LVC1G373 Hi expert,
I just want to know the default outout of SN74LVC1G373.
Before power off ,the output is High.
after power off, if the input signal is low. How about the output signal.
I have seen the function table. but I think it…
Part Number: SN74LVC1G373 Hi team,
Customer wants to know more detailed VOH with Vcc = 1.8V, IOH=-0.3uA. Could you share minimum value? Or customer should understand as 1.7V as minimum value? Because the datasheet shows as below but I don't figure out…
Part Number: SN74LVC1G373 Team,
Customer is choosing SN74LVC1G373 as their logic IC, and they asking what is the output structure of SN74LVC1G373? Open drain or push/pull?
Furthermore, what is the default state of output after IC is waken up from shutdown…