Part Number: SN74LVC1G373
What happens to the output state when the power is turned on again after the latch is powered off? If it is OE=LE=0 as shown in the table below, does it remain in the previous state? I know it is volatile, but it seems to maintain…
Part Number: SN74LVC1G373 Hello expert,
May we know if SN74LVC1G373 could support latch function like when Vin change from high to low, then Vout can keep low no matter Vin high or low change. We can use reset pin to give this latch situation go back to…
Part Number: SN74LVC1G373 Other Parts Discussed in Thread: SN74LVC1G08 , Hi Sir
i want to power button that use SN74LVC1G08 + SN74LVC1G373 to reach my expect waveform.
May you pls help check attached circuit if ok or?
Bogey
Part Number: SN74LVC1G373 Hi team, working with a customer on this device. The datasheet wasn't clear to answer the following:
1. Would the outputs be damaged by a short to ground?
2. And what would the current be limited to?
Part Number: SN74LVC1G373 Other Parts Discussed in Thread: SN74LVC1G14 , SN74LS279A , SN74LVC2G132 Hi,
My customer considers the following circuit.
On this circuit, does this output the following logic waveform, after power-up? Please let me know.
…
Part Number: SN74LVC1G373 Hi,
My customer considers the following circuit.
On this circuit, does this output the following logic waveform, after power-up? Please let me know.
He wants as follows:
When input of D pin moves high to low after power-up…
Part Number: SN74LVC1G373 Other Parts Discussed in Thread: SN74LVC1G175 , TLV809E , SN74LVC1G98 Hello,
Here is my set-up before powering up :
- Vcc and D input are tied together (in 3.3V level)
- LE signal cames from another part (in 3.3V level) and is set…
Part Number: SN74LVC1G373 Hi,
My customer found overshoot on LE pin at D pin Low to High.
Please refer the following waveform.
(CH1; LE, CH2; Q pin)
At they change D pin Low to high, and Q pin become low to high. LE pin has overshoot.
Do the device…