Part Number: SN74LVC1G373 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models You have besides the ibis model also a spice model for this chip. I would be very grateful for the help if you advise how to simulate this chip in…
Part Number: SN74LVC1G373 Other Parts Discussed in Thread: SN74AUP1G74 , SN74AUP1G79 , SN74AUP1G17 , CSD17484F4 , SN74HCS74 , MSP430FR2000 I need to retain a HIGH/LOW state set by MCU (basically, a "bit") while the MCU is in low power (basically off) mode…
Part Number: SN74LVC1G373 I am using SN74LVC1G373, and don't have a need to operate in Hi-Z state. Right now, I am planning to tie !OE to GND.
However, section 8.1 of the datasheet states "To ensure the high-impedance state during power up or power…
Part Number: SN74LVC1G373 Hi team - I am inquiring about Q100 availability for the SN74LVC1G373DBVR . If not available, please make an alternate suggestion. I only need a single channel D-Type Latch.
Thanks,
Scott
Part Number: SN74LVC1G373 Hello,
I am using this part with the following conditions:
OE connected to GND
LE connected to an output signal from a comparator
D connected to VBAT
VBAT = 3.7V
The output of the comparator is also lowpass filtered to prevent…
Part Number: SN74LVC1G373 Hello,
When this latch IC is in it's undefined state (I have found it is most often high), is the device still in push-pull operation? I would like to try to define the undefined state by adding a weak pullup on the output…
Part Number: SN74LVC1G373 What is the output state at power-on for the SN74LVC1G373?
I am starting with the initial conditions of D low and LE low.
I want to guarantee that output Q will be low at start-up, but the datasheet does not say if it will be…