Part Number: SN74LVC1G74 Hi,
I am using SN74LVC1G74RSE in my board and I have some questions that I don't find the answer in the datasheet:
1. When I turn on the device, with the next inputs: PRE_N = 'H' CLR_N = 'H' D = 'H' CLK = 'L'
The output…
Part Number: SN74LVC1G74 Hi All,
I need Transient SPICE model for SN74LVC1G74DCUT for simulation. I have checked in the website but didn't find it anywhere. I could find only Behavioral SPICE model, but I need Transient one.
Please help me to get…
Part Number: SN74LVC1G74 Please tell me about the conditions for clear setting when the power is turned on.
I think that it is necessary to set the PRE terminal to H and the CLR terminal to L to set the clear when the power is turned on.
In this case…
Part Number: SN74LVC1G74 Hi,
Good Day. Customer is operating his existing device for Vcc = 3V and the PRE input for 2.5V. The TI spec he choose has a VIH = 0.65*Vcc and a worst-case of 2V ( Vcc = 3V to 3.6V). Please see the screenshot below. So in his…
Part Number: SN74LVC1G74 Other Parts Discussed in Thread: SN74HCS74 , SN74LVC2G32 , SN74LVC1G97 I saw SN74LVC1G74 can support the power button function as shown in Figure 9-1 in the datasheet.
The circuit is one button that controls one output logic…
Part Number: SN74LVC1G74
we are using SN74LVC1G74 as shown above with this connection.The input to preset i.e..,IMD ERROR SIG1 is 24V,using potential divider circuit it is converted to 3.3V and we are taking output from Q'. It is working properly, like…
Part Number: SN74LVC1G74 Other Parts Discussed in Thread: SN74LVC2G17 , , SN74LVC1G08 Hi sir
Our design is a 19V DC in, so I use the BJT to transfer the voltage to 5V.
And this project need to use the tact switch as the power button,
so we try to…
Part Number: SN74LVC1G74 Other Parts Discussed in Thread: SN74HCS74 Hi,
I am using the part "SN74LVC1G74" in my design. The block diagram is as mentioned below.
CLR#, PRE# and Q is connected to Processor. Q# is not connected. CLK is connected…