Hey Chase,
These logic devices will have no issues with that frequency. I don't support the Gate driver device, I'd recommend going over to the Power management forum to ask that questions on that device.
Part Number: SN74LVC1G99 Other Parts Discussed in Thread: SN74LVC32A , SN74LVC2G00 , SN74HC32 Hi team
Do we have any integrated solution for this logic: CS5=!(!CS*A2*!A1*A0*!RD)?
Thanks,
Cera
Part Number: SN74LVC1G99
My Schematic is as shown above。when I change the input logic of the SN74LVC1G99 PIN C and PIN D,PINY always output low,I've tried several times, I donot konw why。I hope TI engineers can help me solve problems,Thanks very much…
Other Parts Discussed in Thread: SN74LVC1G99 Hello,
i want to use the SN74LVC1G99 as AND logic with 3 State Output.
That means, this truth Table should be valid:
A B C Out
1 1 0 1
So i want to connect A and B with AND logic, and set C as…
Part Number: SN74LVC1G00 Other Parts Discussed in Thread: SN74LVC1G126 , , SN74LVC1G99 Hi
Does TI offer a logic IC that integrates the SN74LVC1G00 and SN74LVC1G126?
Thanks
Part Number: SN74AC3G99 Other Parts Discussed in Thread: SN74LVC1G99 Hi,
I'm replacing various dedicated logic gates in my design with the configurable SN74AC3G99. I need to replace an XNOR gate. On page 11 chapter 7.1, the datasheet mentions that XNOR…
Part Number: SN74LVC1G125 Other Parts Discussed in Thread: SN74LVC1G99 , SN74LVC1G17 Hi experts,
Customer used SN74LVC1G125DCKR and has some questions. To delay the power on/enable timing, they implemented an RC delay on the Enable pin. Since this is…