Part Number: SN74LVC1T45-EP Hi Team,
Please could you share the below to support an ongoing design using SN74LVC1T45MDCKREP:
Junction to Board thermal resistance / Theta jB
Junction to Case thermal resistance / Theta jC
Thanks,
Dan
Part Number: SN74LVC1T45-EP Other Parts Discussed in Thread: SN74LVC1G17-EP I need to drive a 3.3V logic signal 3m on a cable. Can I use this device to translate it to 5V and then re translate it back to 3.3V? It is used not a high speed signal. More…
Part Number: SN74LVC1T45-EP We are using SN74LVC1T45MDCKR-EP in our circuit for driving 5V logic.
There is a question regarding the maximum allowed load capacitance.
What is the maximum load capacitance and if it is a function of frequency, what is…
Part Number: SN74LVC1T45-EP I need to know what the recommended value resistor to use as a pull down or pull up on both data lines. This can be referenced on Page 15 of the data sheet.
Thanks,
Paul
Part Number: SN74LVC1T45-EP Team, can we confirm the below?
I am trying to verify that the normal operating input impedance for the ‘A’ input on the SN74LVC1T45-EP IC is above 100k ohm. Any help with resolving this would be much appreciated…
Part Number: SN74LVC2T45-EP We would like to know R θ(JB) Junction to Board resistance of the Components
SN74LVC2T45MDCTTEP
SN74LVC1T45MDCKREP
Request you share the data ASAP.
Part Number: SN74LVC1T45-EP Other Parts Discussed in Thread: SN74LVC1T45 There is leakage in the VCCA and VCCB power domains for SN74LVC1T45.
if the 74LVC1T45-EP chip has improved this problem, or it still exists?
If there is a buffer with no leakage models…
Part Number: SN74LVC1T45-Q1 Other Parts Discussed in Thread: SN74LVC1T45-EP , Customers are considering SN74LVC1T45-EP in automotive applications. The operating temperature range is from -40°C to 125°C.
There is SN74LVC1T45-Q1 as a similar product…
Hi,
We are currently using the SN74LVC1T45-EP (single-bit dual-supply bus transceiver with configurable voltage translation and 3-state outputs) in one of our designs. Was wondering what short circuit protection is implemented for either A or B output ports…
Part Number: SN74LVC1T45 Other Parts Discussed in Thread: SN74LVC2T45 , Hi team,
Is there a power up sequence for the SN74LVC1T45?
I found guidance on the power-up considerations for the SN74LVC1T45-EP as well as for the SN74LVC2T45.
Please clarify the difference…