Part Number: SN74LVC240A Tool/software: To whom it may concern,
I am reaching out on behalf of my employer to request a letter of volatility (LOV) for part SN74LVC240A. The LOV will be used to develop sanitization procedures for hardware which this…
Part Number: SN74LVC240A Hi team.
My customer got a waveform as bellow.
VCC is 3.3V.
CH1:Out put
CH2:/OEpin
The output is Low when /OE voltage is 1.57V.
According to the data sheet, VIL is 0.8Vmax.
And then, the out put is High when…
Other Parts Discussed in Thread: SN74LVC240A , SN74LV240A SN74LVC240A. Question about the "Output" voltage. Page 11 says the output can not exceed the Vcc which is 3.3v. But, page 1 under Features it says -- Supports Mixed-Mode Signal Operation on All…
Reposting the list of devices with GPNs as the answers wont change between package types or quantity
SN74AC74 SN74AHC1G32 SN74AUP1G99 SN74LVC04A SN74LVC04APWTE4
SN74LVC125A
SN74LVC126A
SN74LVC1G07
SN74LVC1G08
SN74LVC1G14
SN74LVC1G97
SN74LVC1G99…
Hey Howard,
One more question: Are they wanting the output to be 5 V (are they trying to level shift up?)
If not, then you can use the SN74LVC240A/244A as they have a wide operating temp range. They can also be powered from the same 3.3 V rails…
Luke,
Thanks for your answer, it is much appreciated.
I guess I was not clear about the exact type of the board I am using. It is quite old and I am not able to find a direct link on TI site, but the schematics can be found here . The board has UCD9240…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage Translation FAQs - All-Time
How does a slow or floating input affect…