Part Number: SN74LVC2G06 Other Parts Discussed in Thread: SN74HCS05 Do the 74LVC2G06 outputs have clamp diodes going to both GND and VCC rails? Or is it a single diode to ground?
I have a resistor divider node with a 100K resistor going to +43V and…
Part Number: SN74LVC2G06 Other Parts Discussed in Thread: SN74LVC06A , Tool/software: Hello,
Elaborating on the previous thread question, the Absolute Maximum Rating table has a note for VO entries:
"2) The input negative-voltage and output voltage…
Part Number: SN74LVC2G06 Tool/software: Hi
Please help to share the thermal info of the part SN74LVC2G06. Below are the datas we require:
Max Allowed Tj (in degC)
RThetaJC
RThetaJB
Part Number: SN74LVC2G06 Tool/software: What is meant by "Output Clamp Current"?
I would assume that it would be the current through the protection diodes on the output stage, but it is only specified for Vo<0, so I presume that it must be the current…
Part Number: SN74LVC2G06 Other Parts Discussed in Thread: SN74LVC3G06 , SN74LV05A , SN74LV06A Hi team,
Customer is seek Logic IC below condition. Do you have any recommendation?
Vcc=3.3V
Open-drain
multi channel
input L : output HiZ input…
Part Number: SN74LVC2G06 Other Parts Discussed in Thread: UCC21520 , SN74LVC2G04 Hi,
I am testing a PCB that includes a SN74LVC2G06 inverter IC and a gate driver IC UCC21520 to drive two power MOSFETs. The inverter IC is incorporated with associated…