Hello Minglai,
SN74LVC2G06-EP is the generic product name for the EP grade of the part. If you go to that product page or datasheet, you will see that the orderable product name is: SN74LVC2G06MDCKREP or it can be ordered by the VID number: V62/06640…
Part Number: SN74LVC2G06-Q1 Other Parts Discussed in Thread: SN74HCS05-Q1
Hi team,
1. Is there any input clamp diode to clamp the input voltage higher than VCC?
2. Only -Iik is found in D/S. What is the +Iik of this device?
3. There are 6.5~8V…
Part Number: SN74LVC2G06 Hello,
I use the SN74LVC2G06 with 3.3V supply.
The open drain output is pulled up with 4.7k to 5V.
1) Is this connection valid?
2) In this particular connection, will the input voltages correspond to 3.3V? Meanning…
Part Number: SN74LVC2G06 Other Parts Discussed in Thread: SN74LVC2G04 , SN74LVC1G06 Hello Guys,
Good day.
Our customer is looking for the IBIS model for SN74LVC2G06. However this is not available. Can he use the IBIS model from SN74LVC2G04 ?
Is…
Part Number: SN74LVC2G06-Q1 Other Parts Discussed in Thread: SN74LVC1G06 Hi All, Is the IBIS model for SN74LVC2G06-Q1 (Automotive Catalog Dual Inverter Buffer/Driver with Open-Drain Output) available?
Is there any alternate IBIS model which perform…
Part Number: SN74LVC2G06 Hello,
We receive some SN74LVC2G06DCKR with CTJ device marking on it (instead of CT5/CTR)
Do you know if there is an update on this component? Is CTJ a new marking?
Regards
Part Number: SN74LVC2G06 Other Parts Discussed in Thread: SN74AUP2G06 Hello,
I have a battery-run application that requires a signal to be inverted with a circuit that draws a minimum quiescent current. The inverter output shall be open-drain (high…
Part Number: SN74LVC2G06 Team,
Customer is looking at open drain type solution SN74LVC2G06 for 0Vin to 5.5Vout/ 3.3Vin to 0Vout. May I check with you any guideline for the chosen of pull up resistor?
Thanks.
Allan
Other Parts Discussed in Thread: SN74LVC2G06 , SN74LVC1G06 I would like to know if it is possible to get the SN74LVC2G06 Pspice model, as i couldent find it on the part page.
If it is possible please tell me where to get it, or send it via mail.
…