Part Number: SN74LVC2G07 Other Parts Discussed in Thread: SN74LVC2G74 Tool/software: Hi,
Could you please provide the Rjb for VSSOP package?
Thank you
Yishan Chen
Part Number: SN74LVC2G07 Tool/software: Hello,
The buffer part SN74LVC2G07 is considered to be operating at 2.5V. Could you share the VOH, VOL, VIH, VIL voltage levels at 2.5V operation
Part Number: SN74LVC2G07 Tool/software: Hi team,
Could you let me know the θJC value of devices listed below?
SN74LVC2G07DCKT
SN74LVC2G04DCKT
SN74LVC2G06DCKR
My customer is required to investigate θJC internally .
I asked the specific…
Part Number: SN74LVC2G07 Other Parts Discussed in Thread: SN74AC16-Q1 , , SN74LVC2G17 , SN74LVC1G99 Tool/software: Hi,
In our application, we are using the GT-100 integrated circuit (IC), which has a 1.8V reset pin. We plan to reset it using a switch…
Part Number: SN74LVC2G07 Other Parts Discussed in Thread: SN74AUP2G125 , SN74LVC2G125 , SN74AUC2G125 Hi,
We are using the ADC which supports 3 wire SPI communication and we are using SPI level shifter which will convert the 4 wire SPI communication…
Part Number: SN74LVC2G07-EP Tool/software: Hi There,
For the Buffer below, we are expecting around 1 uA of current, what would the respective VOL be?
Thank you! Kara
Part Number: SN74LVC2G07-EP We are using your SN74LVC2G07MDCKTEP part in some boards we are doing thermal analysis on and need additional information that is not in the datasheet. The datasheet lists thermal impedance as 259°C/W but it doesn't say where…
Part Number: SN74LVC2G07 Hi,
For the part SN74LVC2G07DCKT, I am looking for the output capacitance.
The datasheet provides the Ci which is 3.5pF.
But it doesn't provide the output pin + driver capacitance when a steady 3.3V is driven out.
Is it…
Part Number: SN74LVC2G07 Other Parts Discussed in Thread: TXU0102 , SN74LVC2G34 Hi Team,
can the SN74LVC2G07DRY be used to buffer two clock lines that are 5 V level and to convert them to 3.3 V as well?
What is the skew between the two devices? E…