Part Number: SN74LVC2G125 Other Parts Discussed in Thread: SN74LVC2G08 , Hi TI Logic Team,
Just wanted to double check, when the ICs are unpowered, the Ioff feature of eg SN74LVC2G125 and SN74LVC2G08 will prevent the parts to unintentionally be powered…
Part Number: SN74LVC2G08 Hello,
lately we have quality issues concerning the the solder joints of the SN74LVC2G08. We use the package DCT (R-PDSO-G8)
The recommended land pattern for this package is defined as follows.
Our assembly service noted that…
Part Number: SN74LVC1G11 Other Parts Discussed in Thread: SN74AUP2G08 , SN74LVC2G08 , Hi
We are using SN74LVC1G11DRYR in our design. Kindly suggest a equivalent alternate part for this.
Other Parts Discussed in Thread: SN74LVC1G17 , SN74LVC2G08 For the two parts listed, do we need to add decoupling caps near these two devices? The loading is 40pF. Board space is constrained, but in general good bypass practice dictats a bypass cap for…
Other Parts Discussed in Thread: SN74LVC2G08 , CD74AC534 I have another question for you. I use Texas
Instruments SN74LVC2G08. My application is reverse from "Ioff Supports
Partial-Power-Down Mode Operation". VCC power is on, all inputs are in "high…
NAND: SN74LVC2G00 AND: SN74AHC08 (The AHC propagation delay at 3.3 V is marginal. If this is important, use 2× SN74LVC2G08.)
This logic function (AND with one inverted input) could be implemented with just the SN74LVC1G97, but would require four…
Other Parts Discussed in Thread: SN74LVC2G08
HI Apps
Nexperia decided 74LVC2G08GD status change EOL
Do we have Pin compatible sockets for 74LVC2G08GD is made by Nexperia?
Thanks
Yuki
Other Parts Discussed in Thread: SN74HC573A-Q1 , SN74LVC2G08-Q1 Hi,
I just went through these 2 threads from our forum and there are very helpful! Great thanks to Emrys!
https://e2e.ti.com/support/logic/f/151/p/731172/2698649
https://e2e.ti.com/support/logic…
Hi Nathan,
Thank you for the clarification.
In SN74LVC2G08 there is no enable pin. My protection circuit is active High Output so I cant use it directly as the second input of AND gate to disable the pulses.
So do you recommend to pull the output of…