Part Number: SN74LVC2G125 The SN74LVC2G125DCT3 does not have green status for chemicals but the SN74LVC2G125DCTR has.
Seems it is because Bond wire and Lead Frame Plating has not been tested for Halogen. How to get green status on the SN74LVC2G125DCT3…
Part Number: SN74LVC2G125 Other Parts Discussed in Thread: SN74LVC1G125 Tool/software: Under normal circumstances, What is the data rate of SN74LVC2G125? thanks.
Part Number: SN74LVC2G125 Hi Team,
Output connected to GPIO.
GPIO sometimes pulls the SN74LVC2G125's output down to GND
Does the SN74LVC2G125 require a series resistor for current limiting?
If a resistor needs to be placed, what is the recommended…
Part Number: SN74LVC2G125 Hi all,
1) The specified value of Ioz is 10uA. There is no sign for plus or minus. Am I correct in understanding that there are both positive and negative leaks? From the data sheet, Ioz is 10uA only in the positive direction…
Part Number: SN74LVC2G125 Hi Team,
Greetings of the day!
I am Chaithra from Philips component engineer team. I would like to below details for MPN: SN74LVC2G125DCUT which is not able to get it from the datasheet.
Specification:
Power dissipation…
Part Number: SN74LVC2G125 Tool/software: To whom it may concern,
I am reaching out on behalf of my employer to request a letter of volatility (LOV) for part SN74LVC2G125DCUT. The LOV will be used to develop sanitization procedures for hardware which…
Part Number: SN74LVC2G125 Tool/software: Hello,
I would like to use SN74LVC2G125 to provide a buffer on a external UART interface (RX and TX) on a custom PCB design. The issue I have is that the UART signals are 3.0V logic levels and the only power…
Part Number: SN74LVC2G125 Other Parts Discussed in Thread: SN74LV1T125 , SN74AHCT1G125 Dear Team,
I have a question about SN74LVC2G125: OE is L, VCC=5V, when the A port is 3.3V high level, is the Y port a 5V high level?
Many Thanks,
Jimmy
Part Number: SN74LVC2G125 Tool/software: Hello, Order number T04884049 SN74LVC2G125DCTR corresponds to The reference MARKING on the TISTORE PDF data is "2WK5". But the incoming chip is 2WK541K7. What does "41K7" stand for?