Part Number: SN74LVC2G17-Q1 Other Parts Discussed in Thread: SN74HCS244-Q1 For dual Buffer part no. SN74LVC2G17QDCKRQ1, input voltage Vin of 5.5V can be applied, even if VCC is 3.3V, right? Or will Vin_max be 3.3V (same as VCC) only?
Part Number: SN74LVC2G17 As per the buffer datasheet ,Input = Output. But when I checked in hyperlynx tool without giving the input , getting signal at output pin.
Could you please help me to solve this issue.
Part Number: SN74LVC2G17 In IBIS model by default, it’s 1.8V.
This model also support for 3.3V.
Could you pls help to select 3.3V option in IBIS model.
Thank you in Advance.
Part Number: SN74LVC2G17-Q1 Other Parts Discussed in Thread: SN74LVC2G17 Hi Team, There is a good new that Customer is searching TI solution Do we have a product that can compete with "TOSHIBA TC7PZ17FU" ?
the attachment file is TOSHIBA's datasheet…
Part Number: SN74LVC2G17 Hello e2e team,
I am using the SN74LVC2G17 buffer in my design and connected the PWM inputs as follows via the pull down resistor 10k ohm -->
The issue is when I give the supply 3.3V, the pin 2 (of both J17 and J18) both…
Part Number: SN74LVC2G17 Other Parts Discussed in Thread: SN74LVC1G17 Hi Team
Do we have the product with same function as SN74LVC2G17DSF2, but only has one input and one ouput ? THX
Part Number: SN74LVC2G17-Q1 Hi, I am performing Signal Integrity analysis simulation for which I need IBIS model of SN74LVC2G17QDCKRQ1. I looked for same on product 'Design & Development' section but couldn't find it. Please help me to get…
Part Number: SN74LVC2G17-Q1
Hi team,
My customer would like to know power consumption at different working temperature.
May I have your help, thanks.
IC 型號
SN74LVC2G17-Q1
Typ value at +25 ℃
Typ value at +70 ℃
Max value at -4…